Source code for bosdyn.client.graph_nav

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""For clients to the graphnav service."""
import collections
import math
import os
import time

from deprecated.sphinx import deprecated

from bosdyn.api import data_chunk_pb2, lease_pb2
from bosdyn.api.graph_nav import graph_nav_pb2, graph_nav_service_pb2_grpc, map_pb2, nav_pb2
from bosdyn.client.common import (BaseClient, common_header_errors, common_lease_errors,
                                  error_factory, error_pair, handle_common_header_errors,
                                  handle_lease_use_result_errors, handle_license_errors_if_present,
                                  handle_unset_status_error)
from bosdyn.client.exceptions import ResponseError, UnimplementedError
from bosdyn.client.lease import add_lease_wallet_processors
from bosdyn.util import now_sec


[docs]class GraphNavClient(BaseClient): """Client to the GraphNav service.""" default_service_name = 'graph-nav-service' service_type = 'bosdyn.api.graph_nav.GraphNavService' def __init__(self): super(GraphNavClient, self).__init__(graph_nav_service_pb2_grpc.GraphNavServiceStub) self._timesync_endpoint = None self._data_chunk_size = 1024 * 1024 # bytes = 1 MB self._use_streaming_graph_upload = True
[docs] def update_from(self, other): super(GraphNavClient, self).update_from(other) if self.lease_wallet: add_lease_wallet_processors(self, self.lease_wallet) # Grab a timesync endpoint if it is available. try: self._timesync_endpoint = other.time_sync.endpoint except AttributeError: pass # other doesn't have a time_sync accessor
[docs] def set_localization_full_response( self, initial_guess_localization, ko_tform_body=None, max_distance=None, max_yaw=None, fiducial_init=graph_nav_pb2.SetLocalizationRequest.FIDUCIAL_INIT_NEAREST, use_fiducial_id=None, refine_fiducial_result_with_icp=False, do_ambiguity_check=False, refine_with_visual_features=False, verify_visual_features_quality=False, **kwargs): """Version of set_localization which returns the full response, rather than only the Localization message. """ req = self._build_set_localization_request( initial_guess_localization, ko_tform_body, max_distance, max_yaw, fiducial_init, use_fiducial_id, refine_fiducial_result_with_icp, do_ambiguity_check, refine_with_visual_features, verify_visual_features_quality) return self.call(self._stub.SetLocalization, req, _get_response, _set_localization_error, copy_request=False, **kwargs)
[docs] def set_localization_async_full_response( self, initial_guess_localization, ko_tform_body=None, max_distance=None, max_yaw=None, fiducial_init=graph_nav_pb2.SetLocalizationRequest.FIDUCIAL_INIT_NEAREST, use_fiducial_id=None, refine_fiducial_result_with_icp=False, do_ambiguity_check=False, refine_with_visual_features=False, verify_visual_features_quality=False, **kwargs): """Async version of set_localization_full_response()""" req = self._build_set_localization_request( initial_guess_localization, ko_tform_body, max_distance, max_yaw, fiducial_init, use_fiducial_id, refine_fiducial_result_with_icp, do_ambiguity_check, refine_with_visual_features, verify_visual_features_quality) return self.call_async(self._stub.SetLocalization, req, _get_response, _set_localization_error, copy_request=False, **kwargs)
[docs] def set_localization( self, initial_guess_localization, ko_tform_body=None, max_distance=None, max_yaw=None, fiducial_init=graph_nav_pb2.SetLocalizationRequest.FIDUCIAL_INIT_NEAREST, use_fiducial_id=None, refine_fiducial_result_with_icp=False, do_ambiguity_check=False, refine_with_visual_features=False, verify_visual_features_quality=False, **kwargs): """Trigger a manual localization. Typically done to provide the initial localization. Args: initial_guess_localization (nav_pb2.Localization): Operator-supplied guess at localization. ko_tform_body: Robot SE3Pose protobuf when the initial_guess was made. max_distance: [optional] Margin of distance (meters) away from the initial guess. max_yaw: [optional] Margin of angle (radians) away from the initial guess. fiducial_init: Tells the initializer whether to use fiducials, and how to use them. use_fiducial_id: If using FIDUCIAL_INIT_SPECIFIC, this is the specific fiducial ID to use for initialization. refine_fiducial_result_with_icp: Boolean determining if ICP will run after a fiducial is used for an initial guess. do_ambiguity_check: Boolean where if true, consider how nearby localizations appear. refine_with_visual_features: Boolean determining if visual features should be used to refine the estimate. When set, this value overrides refine_fiducial_result_with_icp. verify_visual_features_quality: When refine_with_visual_features is set, determines if an error is asserted when the refinement is unsuccessful. Returns: The resulting localization after being triggered with a guess. Raises: RpcError: Problem communicating with the robot RobotFaultedError: Robot is experiencing a fault condition that prevents localization. UnknownMapInformationError: Specified waypoint is unknown. bosdyn.client.exceptions.InvalidRequestError: The data provided is incomplete or invalid GraphNavServiceResponseError: Localization was aborted or failed. """ req = self._build_set_localization_request( initial_guess_localization, ko_tform_body, max_distance, max_yaw, fiducial_init, use_fiducial_id, refine_fiducial_result_with_icp, do_ambiguity_check, refine_with_visual_features, verify_visual_features_quality) return self.call(self._stub.SetLocalization, req, _localization_from_response, _set_localization_error, copy_request=False, **kwargs)
[docs] def set_localization_async( self, initial_guess_localization, ko_tform_body=None, max_distance=None, max_yaw=None, fiducial_init=graph_nav_pb2.SetLocalizationRequest.FIDUCIAL_INIT_NEAREST, use_fiducial_id=None, refine_fiducial_result_with_icp=False, do_ambiguity_check=False, refine_with_visual_features=False, verify_visual_features_quality=False, **kwargs): """Async version of set_localization()""" req = self._build_set_localization_request( initial_guess_localization, ko_tform_body, max_distance, max_yaw, fiducial_init, use_fiducial_id, refine_fiducial_result_with_icp, do_ambiguity_check, refine_with_visual_features, verify_visual_features_quality) return self.call_async(self._stub.SetLocalization, req, _localization_from_response, _set_localization_error, copy_request=False, **kwargs)
[docs] def get_localization_state( self, request_live_point_cloud=False, request_live_images=False, request_live_terrain_maps=False, request_live_world_objects=False, request_live_robot_state=False, waypoint_id=None, request_gps_state=False, **kwargs): """Obtain current localization state of the robot. Returns: The current localization protobuf for the robot. Raises: RpcError: Problem communicating with the robot. """ req = self._build_get_localization_state_request( request_live_point_cloud=request_live_point_cloud, request_live_images=request_live_images, request_live_terrain_maps=request_live_terrain_maps, request_live_world_objects=request_live_world_objects, request_live_robot_state=request_live_robot_state, waypoint_id=waypoint_id, request_gps_state=request_gps_state) return self.call(self._stub.GetLocalizationState, req, None, common_header_errors, copy_request=False, **kwargs)
[docs] def get_localization_state_async( self, request_live_point_cloud=False, request_live_images=False, request_live_terrain_maps=False, request_live_world_objects=False, request_live_robot_state=False, waypoint_id=None, request_gps_state=False, **kwargs): """Async version of get_localization_state().""" req = self._build_get_localization_state_request( request_live_point_cloud=request_live_point_cloud, request_live_images=request_live_images, request_live_terrain_maps=request_live_terrain_maps, request_live_world_objects=request_live_world_objects, request_live_robot_state=request_live_robot_state, waypoint_id=waypoint_id, request_gps_state=request_gps_state) return self.call_async(self._stub.GetLocalizationState, req, None, common_header_errors, copy_request=False, **kwargs)
[docs] def navigate_route(self, route, cmd_duration, route_follow_params=None, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, **kwargs): """Navigate the given route. Args: route: Route protobuf of the route to follow. route_follow_params: What should the robot do if it is not at the expected point in the route, or the route is blocked. travel_params: API TravelParams for the route. cmd_duration: Number of seconds the command can run for. leases: Leases to show ownership of necessary resources. Will use the client's leases by default. timesync_endpoint: Use this endpoint for timesync fields. Will use the client's endpoint by default. command_id: If not None, this continues an existing navigate_route command with the given ID. If None, a new command_id will be used. destination_waypoint_tform_body_goal: SE2Pose protobuf of an offset relative to the destination waypoint. kwargs: Passed to underlying RPC. Example: timeout=5 to cancel the RPC after 5 seconds. Returns: Command ID to use in feedback lookup. Raises: RpcError: Problem communicating with the robot. LeaseUseError: Error using provided leases. graph_nav.NoTimeSyncError: Missing clock identifier. graph_nav.CommandExpiredError: Command already expired. graph_nav.TooDistantError: Time too far in the future. graph_nav.RobotImpairedError: Robot cannot travel a route. graph_nav.IsRecordingError: Robot cannot navigate while recording. graph_nav.UnknownRouteElementsError: Unknown edges or waypoints graph_nav.InvalidEdgeError: Mismatch between edges and waypoints. graph_nav.NoPathError: No path to the specified route. graph_nav.RobotNotLocalizedToRouteError: The robot is localized somewhere else. graph_nav.ConstraintFaultError: The route involves invalid constraints. graph_nav.RouteNavigationError: A subclass detailing trouble navigating the route. """ used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_route_request(route, route_follow_params, travel_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal) return self.call(self._stub.NavigateRoute, request, _command_id_from_navigate_route_response, _navigate_route_error, copy_request=False, **kwargs)
[docs] def navigate_route_async(self, route, cmd_duration, route_follow_params=None, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, **kwargs): """Async version of navigate_route()""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_route_request(route, route_follow_params, travel_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal) return self.call_async(self._stub.NavigateRoute, request, _command_id_from_navigate_route_response, _navigate_route_error, copy_request=False, **kwargs)
[docs] def navigate_route_full(self, route, route_follow_params, cmd_duration, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, **kwargs): """Identical to navigate_route(), except will return the full NavigateRouteResponse.""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_route_request(route, route_follow_params, travel_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal) return self.call(self._stub.NavigateRoute, request, error_from_response=_navigate_route_error, copy_request=False, **kwargs)
[docs] def navigate_route_full_async( self, route, cmd_duration, route_follow_params=None, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, **kwargs): """Async version of navigate_route_full().""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_route_request( route, route_follow_params, travel_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal, ) return self.call_async(self._stub.NavigateRoute, request, error_from_response=_navigate_route_error, copy_request=False, **kwargs)
[docs] def navigate_to(self, destination_waypoint_id, cmd_duration, route_params=None, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, route_blocked_behavior=None, **kwargs): """Navigate to a specific waypoint along a route chosen by the GraphNav service. Args: destination_waypoint_id: Waypoint id string for where to go to. cmd_duration: Number of seconds the command can run for. route_params: API RouteGenParams for the route. travel_params: API TravelParams for the route. leases: Leases to show ownership of necessary resources. Will use the client's leases by default. timesync_endpoint: Use this endpoint for timesync fields. Will use the client's endpoint by default. command_id: If not None, this continues an existing navigate_to command with the given ID. If None, a new command_id will be used. destination_waypoint_tform_body_goal: SE2Pose protobuf of an offset relative to the destination waypoint. route_blocked_behavior: Defines robot behavior when route is block. If None robot will reroute. Returns: int: Command ID to use in feedback lookup. Raises: RpcError: Problem communicating with the robot. LeaseUseError: Error using provided leases. graph_nav.NoTimeSyncError: Missing clock identifier. graph_nav.CommandExpiredError: Command already expired. graph_nav.TooDistantError: Time too far in the future. graph_nav.RobotImpairedError: Robot cannot travel a route. graph_nav.IsRecordingError: Robot cannot navigate while recording. graph_nav.UnknownWaypointError: Destination waypoint is unknown. graph_nav.NoPathError: No route to destination. graph_nav.RobotNotLocalizedToRouteError: The robot not correctly localized. graph_nav.RouteNavigationError: A subclass detailing trouble navigating the route. """ used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_to_request(destination_waypoint_id, travel_params, route_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal, route_blocked_behavior) return self.call(self._stub.NavigateTo, request, value_from_response=_command_id_from_navigate_route_response, error_from_response=_navigate_to_error, copy_request=False, **kwargs)
[docs] def navigate_to_async(self, destination_waypoint_id, cmd_duration, route_params=None, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, route_blocked_behavior=None, **kwargs): """Async version of navigate_to().""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_to_request(destination_waypoint_id, travel_params, route_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal, route_blocked_behavior) return self.call_async(self._stub.NavigateTo, request, value_from_response=_command_id_from_navigate_route_response, error_from_response=_navigate_to_error, copy_request=False, **kwargs)
[docs] def navigate_to_full(self, destination_waypoint_id, cmd_duration, route_params=None, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, route_blocked_behavior=None, **kwargs): """Identical to navigate_to(), except will return the full NavigateToResponse.""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_to_request(destination_waypoint_id, travel_params, route_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal, route_blocked_behavior) return self.call(self._stub.NavigateTo, request, error_from_response=_navigate_to_error, copy_request=False, **kwargs)
[docs] def navigate_to_full_async(self, destination_waypoint_id, cmd_duration, route_params=None, travel_params=None, leases=None, timesync_endpoint=None, command_id=None, destination_waypoint_tform_body_goal=None, route_blocked_behavior=None, **kwargs): """Async version of navigate_to_full().""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_to_request(destination_waypoint_id, travel_params, route_params, cmd_duration, leases, used_endpoint, command_id, destination_waypoint_tform_body_goal, route_blocked_behavior) return self.call_async(self._stub.NavigateTo, request, error_from_response=_navigate_to_error, copy_request=False, **kwargs)
[docs] def navigate_to_anchor(self, seed_tform_goal, cmd_duration, route_params=None, travel_params=None, leases=None, timesync_endpoint=None, goal_waypoint_rt_seed_ewrt_seed_tolerance=None, command_id=None, gps_navigation_params=None, **kwargs): """Navigate to a pose in seed frame along a route chosen by the GraphNav service. Args: seed_tform_goal: SE3Pose protobuf of the goal pose in seed frame. cmd_duration: Number of seconds the command can run for. route_params: API RouteGenParams for the route. travel_params: API TravelParams for the route. leases: Leases to show ownership of necessary resources. Will use the client's leases by default. timesync_endpoint: Use this endpoint for timesync fields. Will use the client's endpoint by default. goal_waypoint_rt_seed_ewrt_seed_tolerance: Vec3 protobuf of the tolerances for goal waypoint selection. command_id: If not None, this continues an existing navigate_to command with the given ID. If None, a new command_id will be used. gps_navigation_params: API GPSNavigationParams. If not None, this will be interpreted as a GPS-based navigation command. seed_tform_goal will be ignored and whatever goal is passed in using the GPS navigation params will be used. Returns: int: Command ID to use in feedback lookup. Raises: RpcError: Problem communicating with the robot. LeaseUseError: Error using provided leases. graph_nav.NoTimeSyncError: Missing clock identifier. graph_nav.CommandExpiredError: Command already expired. graph_nav.TooDistantError: Time too far in the future. graph_nav.RobotImpairedError: Robot cannot travel a route. graph_nav.IsRecordingError: Robot cannot navigate while recording. graph_nav.NoAnchoringError: There is no anchoring. graph_nav.NoPathError: No route to goal waypoint, or no goal waypoint found. graph_nav.InvalidPoseError: The requested pose is invalid, or known to be unachievable. graph_nav.RobotNotLocalizedToRouteError: The robot not correctly localized. graph_nav.RouteNavigationError: A subclass detailing trouble navigating the route. """ used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_to_anchor_request( seed_tform_goal, travel_params, route_params, cmd_duration, leases, used_endpoint, command_id, goal_waypoint_rt_seed_ewrt_seed_tolerance, gps_navigation_params) return self.call(self._stub.NavigateToAnchor, request, value_from_response=_command_id_from_navigate_route_response, error_from_response=_navigate_to_anchor_error, copy_request=False, **kwargs)
[docs] def navigate_to_anchor_async(self, seed_tform_goal, cmd_duration, route_params=None, travel_params=None, leases=None, timesync_endpoint=None, goal_waypoint_rt_seed_ewrt_seed_tolerance=None, command_id=None, gps_navigation_params=None, **kwargs): """Async version of navigate_to_anchor().""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_to_anchor_request( seed_tform_goal, travel_params, route_params, cmd_duration, leases, used_endpoint, command_id, goal_waypoint_rt_seed_ewrt_seed_tolerance, gps_navigation_params) return self.call_async(self._stub.NavigateToAnchor, request, value_from_response=_command_id_from_navigate_route_response, error_from_response=_navigate_to_anchor_error, copy_request=False, **kwargs)
[docs] def navigate_to_anchor_full_async(self, seed_tform_goal, cmd_duration, route_params=None, travel_params=None, leases=None, timesync_endpoint=None, goal_waypoint_rt_seed_ewrt_seed_tolerance=None, command_id=None, gps_navigation_params=None, **kwargs): """Async version of navigate_to_anchor() that returns the full response.""" used_endpoint = timesync_endpoint or self._timesync_endpoint if not used_endpoint: raise GraphNavServiceResponseError(response=None, error_message='No timesync endpoint!') request = self._build_navigate_to_anchor_request( seed_tform_goal, travel_params, route_params, cmd_duration, leases, used_endpoint, command_id, goal_waypoint_rt_seed_ewrt_seed_tolerance, gps_navigation_params) return self.call_async(self._stub.NavigateToAnchor, request, error_from_response=_navigate_to_anchor_error, copy_request=False, **kwargs)
[docs] def navigation_feedback(self, command_id=0, **kwargs): """Returns the feedback corresponding to the active route follow command. Args: command_id (int): If blank, will return current command status. If filled out, will attempt to return that command status Returns: NavigationFeedbackResponse Raises: RpcError: Problem communicating with the robot. """ request = self._build_navigate_feedback_request(command_id) return self.call(self._stub.NavigationFeedback, request, value_from_response=_get_response, error_from_response=_navigate_feedback_error, copy_request=False, **kwargs)
[docs] def navigation_feedback_async(self, command_id=0, **kwargs): """Async version of navigation_feedback().""" request = self._build_navigate_feedback_request(command_id) return self.call_async(self._stub.NavigationFeedback, request, value_from_response=_get_response, error_from_response=_navigate_feedback_error, copy_request=False, **kwargs)
[docs] def clear_graph(self, lease=None, **kwargs): """Clears the local graph structure. Also erases any snapshots currently in RAM. Args: lease: Leases to show ownership of necessary resources. Will use the client's leases by default. Raises: RpcError: Problem communicating with the robot. LeaseUseError: Error using provided lease. """ request = self._build_clear_graph_request(lease) return self.call(self._stub.ClearGraph, request, value_from_response=None, error_from_response=_clear_graph_error, copy_request=False, **kwargs)
[docs] def clear_graph_async(self, lease=None, **kwargs): """Async version of clear_graph().""" request = self._build_clear_graph_request(lease) return self.call_async(self._stub.ClearGraph, request, value_from_response=None, error_from_response=handle_common_header_errors(common_lease_errors), copy_request=False, **kwargs)
[docs] def upload_graph(self, lease=None, graph=None, generate_new_anchoring=False, replace_graph=False, **kwargs): """Uploads a graph to the server and appends to the existing graph. Args: lease: Leases to show ownership of necessary resources. Will use the client's leases by default. graph: Graph protobuf that represents the map with waypoints and edges. generate_new_anchoring: Whether to generate an (overwrite the) anchoring on upload. replace_graph: If true, replaces the existing graph with the new one rather than adding to it. Returns: The response, which includes waypoint and edge id's sorted by whether it was cached. Raises: RpcError: Problem communicating with the robot. UploadGraphError: Indicates a problem with the map provided. IncompatibleSensorsError: The map was recorded with different sensors than the robot. AreaCallbackError: The map includes area callback services not present on the robot. LeaseUseError: Error using provided lease. LicenseError: The robot's license is not valid. """ request = self._build_upload_graph_request(lease, graph, generate_new_anchoring, replace_graph) # Use streaming to upload the graph, if applicable. if self._use_streaming_graph_upload: # Need to manually apply request processors since this will be serialized and chunked. self._apply_request_processors(request, copy_request=False) serialized = request.SerializeToString() try: return self.call( self._stub.UploadGraphStreaming, GraphNavClient._data_chunk_iterator_upload_graph(serialized, self._data_chunk_size), value_from_response=_get_response, error_from_response=_upload_graph_error, **kwargs) except UnimplementedError: print('UploadGraphStreaming unimplemented. Old robot release?') # Recreate the request so that we clear any state that might have happened during our attempt to stream. request = self._build_upload_graph_request(lease, graph, generate_new_anchoring, replace_graph) # Continue to regular UploadGraph. return self.call(self._stub.UploadGraph, request, value_from_response=_get_response, error_from_response=_upload_graph_error, copy_request=False, **kwargs)
[docs] def upload_graph_async(self, lease=None, graph=None, generate_new_anchoring=False, replace_graph=False, **kwargs): """Async version of upload_graph().""" request = self._build_upload_graph_request(lease, graph, generate_new_anchoring, replace_graph) return self.call_async(self._stub.UploadGraph, request, value_from_response=_get_response, error_from_response=_upload_graph_error, copy_request=False, **kwargs)
[docs] def upload_waypoint_snapshot(self, waypoint_snapshot, lease=None, **kwargs): """Uploads large waypoint snapshot as a stream for a particular waypoint. Args: lease: Leases to show ownership of necessary resources. Will use the client's leases by default. waypoint_snapshot: WaypointSnapshot protobuf that will be stream-uploaded to the robot. Returns: The status of the upload request. Raises: RpcError: Problem communicating with the robot. LeaseUseError: Error using provided lease. """ lease = lease or lease_pb2.Lease() serialized = waypoint_snapshot.SerializeToString() self.call( self._stub.UploadWaypointSnapshot, GraphNavClient._data_chunk_iterator_upload_waypoint_snapshot( serialized, lease, self._data_chunk_size), value_from_response=None, error_from_response=_upload_waypoint_snapshot_error, **kwargs)
[docs] def upload_edge_snapshot(self, edge_snapshot, lease=None, **kwargs): """Uploads large edge snapshot as a stream for a particular edge. Args: lease: Leases to show ownership of necessary resources. Will use the client's leases by default. edge_snapshot: EdgeSnapshot protobuf that will be stream-uploaded to the robot. Returns: The status of the upload request. Raises: RpcError: Problem communicating with the robot. LeaseUseError: Error using provided leases. """ lease = lease or lease_pb2.Lease() serialized = edge_snapshot.SerializeToString() self.call( self._stub.UploadEdgeSnapshot, GraphNavClient._data_chunk_iterator_upload_edge_snapshot(serialized, lease, self._data_chunk_size), value_from_response=None, error_from_response=handle_common_header_errors(common_lease_errors), **kwargs)
[docs] def upload_snapshots(self, snapshots, lease=None, **kwargs): """Uploads multiple snapshots as a stream. graph_nav only processes complete Snapshots so large protos are discouraged; any network interruption would require the data to be resent. Clients are encouraged to send data in batches on the order of a few MB to strike a balance between eliminating per-RPC overhead and recovering from errors. Args: lease: Leases to show ownership of necessary resources. Will use the client's leases by default. snapshots: UploadSnapshotsRequest.Snapshots protobuf that will be stream-uploaded to the robot. Returns: The status of the upload request. Raises: RpcError: Problem communicating with the robot. LeaseUseError: Error using provided leases. """ lease = lease or lease_pb2.Lease() serialized = snapshots.SerializeToString() self.call( self._stub.UploadSnapshots, GraphNavClient._data_chunk_iterator_upload_snapshots(serialized, lease, self._data_chunk_size), value_from_response=None, error_from_response=handle_common_header_errors(common_lease_errors), **kwargs)
[docs] def download_graph(self, **kwargs): """Downloads the graph from the server. Returns: The graph protobuf that represents the current map on the robot (with waypoints and edges). Raises: RpcError: Problem communicating with the robot """ request = self._build_download_graph_request() # Use streaming to download the graph, if applicable. if self._use_streaming_graph_upload: try: resp = self.call(self._stub.DownloadGraphStreaming, request, value_from_response=_get_streamed_download_graph, error_from_response=_download_graph_stream_errors, copy_request=False, **kwargs) return resp except UnimplementedError: print('DownloadGraphStreaming unimplemented. Old robot release?') # Continue to regular DownloadGraph. return self.call(self._stub.DownloadGraph, request, value_from_response=_get_graph, error_from_response=common_header_errors, copy_request=False, **kwargs)
[docs] def download_graph_async(self, **kwargs): """Async version of download_graph().""" request = self._build_download_graph_request() return self.call_async(self._stub.DownloadGraph, request, value_from_response=_get_graph, error_from_response=common_header_errors, copy_request=False, **kwargs)
[docs] def download_waypoint_snapshot( self, waypoint_snapshot_id, download_images=False, do_not_download_point_cloud=False, **kwargs): """Download a specific waypoint snapshot with streaming from the server. Args: waypoint_snapshot_id: WaypointSnapshot string ID for which snapshot to download from robot. download_images: Boolean indicating whether to include images in the download. do_not_download_point_cloud: Boolean indicating if point cloud data should not be downloaded. Returns: The WaypointSnapshot protobuf from the robot's current map. Raises: RpcError: Problem communicating with the robot UnknownMapInformationError: Snapshot id not found """ request = self._build_download_waypoint_snapshot_request( waypoint_snapshot_id, download_images, do_not_download_point_cloud) return self.call(self._stub.DownloadWaypointSnapshot, request, value_from_response=_get_streamed_waypoint_snapshot, error_from_response=_download_waypoint_snapshot_stream_errors, copy_request=False, **kwargs)
[docs] def download_edge_snapshot(self, edge_snapshot_id, **kwargs): """Downloads a specific edge snapshot with streaming from the server. Args: edge_snapshot_id: EdgeSnapshot string ID for which snapshot to download from robot. Returns: The EdgeSnapshot protobuf from the robot's current map. Raises: RpcError: Problem communicating with the robot UnknownMapInformationError: Snapshot id not found """ request = self._build_download_edge_snapshot_request(edge_snapshot_id) return self.call(self._stub.DownloadEdgeSnapshot, request, value_from_response=_get_streamed_edge_snapshot, error_from_response=_download_edge_snapshot_stream_errors, copy_request=False, **kwargs)
def _write_bytes(self, filepath, filename, data): """Write data to a file.""" os.makedirs(filepath, exist_ok=True) with open(filepath + filename, 'wb+') as f: f.write(data) f.close()
[docs] def write_graph_and_snapshots(self, directory): """Download the graph and snapshots from robot to the specified directory.""" graph = self.download_graph() graph_bytes = graph.SerializeToString() self._write_bytes(directory, '/graph', graph_bytes) for waypoint in graph.waypoints: if len(waypoint.snapshot_id) == 0: continue waypoint_snapshot = self.download_waypoint_snapshot(waypoint.snapshot_id) self._write_bytes(directory + '/waypoint_snapshots', '/' + waypoint.snapshot_id, waypoint_snapshot.SerializeToString()) for edge in graph.edges: if len(edge.snapshot_id) == 0: continue edge_snapshot = self.download_edge_snapshot(edge.snapshot_id) self._write_bytes(directory + '/edge_snapshots', '/' + edge.snapshot_id, edge_snapshot.SerializeToString())
@staticmethod def _build_set_localization_request( initial_guess_localization, ko_tform_body=None, max_distance=None, max_yaw=None, fiducial_init=graph_nav_pb2.SetLocalizationRequest.FIDUCIAL_INIT_NEAREST, use_fiducial_id=None, refine_fiducial_result_with_icp=False, do_ambiguity_check=False, refine_with_visual_features=False, verify_visual_features_quality=False): request = graph_nav_pb2.SetLocalizationRequest(fiducial_init=fiducial_init) request.initial_guess.CopyFrom(initial_guess_localization) if ko_tform_body is not None: request.ko_tform_body.CopyFrom(ko_tform_body) if max_distance is not None: request.max_distance = max_distance if max_yaw is not None: request.max_yaw = max_yaw if (fiducial_init == graph_nav_pb2.SetLocalizationRequest.FIDUCIAL_INIT_SPECIFIC): if use_fiducial_id is not None: request.use_fiducial_id = use_fiducial_id if refine_with_visual_features: request.refine_with_visual_features.verify_refinement_quality = verify_visual_features_quality elif refine_fiducial_result_with_icp: request.refine_fiducial_result_with_icp = refine_fiducial_result_with_icp request.do_ambiguity_check = do_ambiguity_check return request @staticmethod def _build_get_localization_state_request(request_live_point_cloud, request_live_images, request_live_terrain_maps, request_live_world_objects, request_live_robot_state, waypoint_id, request_gps_state): return graph_nav_pb2.GetLocalizationStateRequest( request_live_point_cloud=request_live_point_cloud, request_live_images=request_live_images, request_live_terrain_maps=request_live_terrain_maps, request_live_world_objects=request_live_world_objects, request_live_robot_state=request_live_robot_state, waypoint_id=waypoint_id, request_gps_state=request_gps_state) @staticmethod def _build_navigate_route_request( route, route_follow_params, travel_params, end_time_secs, leases, timesync_endpoint, command_id, destination_waypoint_tform_body_goal, ): converter = timesync_endpoint.get_robot_time_converter() request = graph_nav_pb2.NavigateRouteRequest( route=route, route_follow_params=route_follow_params, destination_waypoint_tform_body_goal=destination_waypoint_tform_body_goal, clock_identifier=timesync_endpoint.clock_identifier) if travel_params is not None: request.travel_params.CopyFrom(travel_params) request.end_time.CopyFrom( converter.robot_timestamp_from_local_secs(now_sec() + end_time_secs)) if command_id is not None: request.command_id = command_id return request @staticmethod def _build_navigate_to_request(destination_waypoint_id, travel_params, route_params, end_time_secs, leases, timesync_endpoint, command_id, destination_waypoint_tform_body_goal, route_blocked_behavior): converter = timesync_endpoint.get_robot_time_converter() request = graph_nav_pb2.NavigateToRequest( destination_waypoint_id=destination_waypoint_id, destination_waypoint_tform_body_goal=destination_waypoint_tform_body_goal, clock_identifier=timesync_endpoint.clock_identifier) request.end_time.CopyFrom( converter.robot_timestamp_from_local_secs(now_sec() + end_time_secs)) if travel_params is not None: request.travel_params.CopyFrom(travel_params) if route_params is not None: request.route_params.CopyFrom(route_params) if command_id is not None: request.command_id = command_id if route_blocked_behavior is not None: request.route_blocked_behavior = route_blocked_behavior return request @staticmethod def _build_navigate_to_anchor_request(seed_tform_goal, travel_params, route_params, end_time_secs, leases, timesync_endpoint, command_id, goal_waypoint_rt_seed_ewrt_seed_tolerance, gps_navigation_params): converter = timesync_endpoint.get_robot_time_converter() request = graph_nav_pb2.NavigateToAnchorRequest( seed_tform_goal=seed_tform_goal, goal_waypoint_rt_seed_ewrt_seed_tolerance=goal_waypoint_rt_seed_ewrt_seed_tolerance, clock_identifier=timesync_endpoint.clock_identifier) # Note that this overrides the seed_tform_goal, which is a OneOf. if gps_navigation_params: request.gps_navigation_params.CopyFrom(gps_navigation_params) request.end_time.CopyFrom( converter.robot_timestamp_from_local_secs(now_sec() + end_time_secs)) if travel_params is not None: request.travel_params.CopyFrom(travel_params) if route_params is not None: request.route_params.CopyFrom(route_params) if command_id is not None: request.command_id = command_id return request @staticmethod def _build_clear_graph_request(lease): lease = lease or lease_pb2.Lease() return graph_nav_pb2.ClearGraphRequest(lease=lease) @staticmethod def _build_navigate_feedback_request(command_id=0): return graph_nav_pb2.NavigationFeedbackRequest(command_id=command_id) @staticmethod def _build_upload_graph_request(lease, graph, generate_new_anchoring, replace_graph): lease = lease or lease_pb2.Lease() return graph_nav_pb2.UploadGraphRequest(lease=lease, graph=graph, generate_new_anchoring=generate_new_anchoring, replace_graph=replace_graph) @staticmethod def _data_chunk_iterator_upload_graph(serialized_upload_graph, data_chunk_byte_size): """Converts a serialized UploadGraphRequest into a series of UploadGraphStreamingRequests.""" total_bytes_size = len(serialized_upload_graph) num_chunks = math.ceil(total_bytes_size / data_chunk_byte_size) for i in range(num_chunks): start_index = i * data_chunk_byte_size end_index = (i + 1) * data_chunk_byte_size chunk = data_chunk_pb2.DataChunk(total_size=total_bytes_size) if (end_index > total_bytes_size): chunk.data = serialized_upload_graph[start_index:total_bytes_size] else: chunk.data = serialized_upload_graph[start_index:end_index] req = graph_nav_pb2.UploadGraphStreamingRequest(chunk=chunk) yield req @staticmethod def _data_chunk_iterator_upload_waypoint_snapshot(serialized_waypoint_snapshot, lease, data_chunk_byte_size): total_bytes_size = len(serialized_waypoint_snapshot) num_chunks = math.ceil(total_bytes_size / data_chunk_byte_size) for i in range(num_chunks): start_index = i * data_chunk_byte_size end_index = (i + 1) * data_chunk_byte_size chunk = data_chunk_pb2.DataChunk(total_size=total_bytes_size) if (end_index > total_bytes_size): chunk.data = serialized_waypoint_snapshot[start_index:total_bytes_size] else: chunk.data = serialized_waypoint_snapshot[start_index:end_index] req = graph_nav_pb2.UploadWaypointSnapshotRequest(lease=lease, chunk=chunk) yield req @staticmethod def _data_chunk_iterator_upload_edge_snapshot(serialized_edge_snapshot, lease, data_chunk_byte_size): total_bytes_size = len(serialized_edge_snapshot) num_chunks = math.ceil(total_bytes_size / data_chunk_byte_size) for i in range(num_chunks): start_index = i * data_chunk_byte_size end_index = (i + 1) * data_chunk_byte_size chunk = data_chunk_pb2.DataChunk(total_size=total_bytes_size) if (end_index > total_bytes_size): chunk.data = serialized_edge_snapshot[start_index:total_bytes_size] else: chunk.data = serialized_edge_snapshot[start_index:end_index] req = graph_nav_pb2.UploadEdgeSnapshotRequest(lease=lease, chunk=chunk) yield req @staticmethod def _data_chunk_iterator_upload_snapshots(serialized_snapshots, lease, data_chunk_byte_size): total_bytes_size = len(serialized_snapshots) # If the snapshots are empty, still send one empty request. # This is used to probe if the RPC is implemented. if 0 == total_bytes_size: req = graph_nav_pb2.UploadSnapshotsRequest(lease=lease) yield req num_chunks = math.ceil(total_bytes_size / data_chunk_byte_size) for i in range(num_chunks): start_index = i * data_chunk_byte_size end_index = (i + 1) * data_chunk_byte_size chunk = data_chunk_pb2.DataChunk(total_size=total_bytes_size) if (end_index > total_bytes_size): chunk.data = serialized_snapshots[start_index:total_bytes_size] else: chunk.data = serialized_snapshots[start_index:end_index] req = graph_nav_pb2.UploadSnapshotsRequest(lease=lease, chunk=chunk) yield req @staticmethod def _build_download_graph_request(): return graph_nav_pb2.DownloadGraphRequest() @staticmethod def _build_download_waypoint_snapshot_request( waypoint_snapshot_id, download_images, do_not_download_point_cloud=False): return graph_nav_pb2.DownloadWaypointSnapshotRequest( waypoint_snapshot_id=waypoint_snapshot_id, download_images=download_images, do_not_download_point_cloud=do_not_download_point_cloud) @staticmethod def _build_download_edge_snapshot_request(edge_snapshot_id): return graph_nav_pb2.DownloadEdgeSnapshotRequest(edge_snapshot_id=edge_snapshot_id)
[docs] @staticmethod def generate_travel_params(max_distance, max_yaw, velocity_limit=None): """ Generate the API TravelParams for navigation requests. Args: max_distance: Distances (meters) threshold for when we've reached the final waypoint. max_yaw: Angle (radians) threshold for when we've reached the final waypoint. velocity_limit: SE2VelocityLimit protobuf message for the speed the robot should use. Returns: The API TravelParams protobuf message. """ travel_params = graph_nav_pb2.TravelParams(max_distance=max_distance, max_yaw=max_yaw) if velocity_limit is not None: travel_params.velocity_limit.CopyFrom(velocity_limit) return travel_params
[docs] @staticmethod def build_route(waypoint_id_list, edge_id_list): """ Generate the API Route for navigation requests. Args: waypoint_id_list: List of waypoint id strings in which a route should pass through. The ids should be ordered from [start waypoint --> destination waypoint]. edge_id_list: List of the edge_id's which should be in the same ordering as the waypoint list. Returns: The API Route protobuf message. """ route = nav_pb2.Route() route.waypoint_id.extend(waypoint_id_list) route.edge_id.extend(edge_id_list) return route
''' Static helper methods for handing responses and errors. '''
[docs]class GraphNavServiceResponseError(ResponseError): """General class of errors for the GraphNav Recording Service."""
[docs]class UploadWaypointSnapshotError(GraphNavServiceResponseError): """Errors related to uploading a waypoint snapshot"""
[docs]class UploadGraphError(GraphNavServiceResponseError): """Errors related to uploading a graph."""
[docs]class MapTooLargeLicenseError(UploadGraphError): """The map is too large for the license on the robot."""
[docs]class InvalidGraphError(UploadGraphError): """The graph is invalid topologically, e.g. missing waypoints referenced by edges."""
[docs]class IncompatibleSensorsError(GraphNavServiceResponseError): """The map was recorded with using a sensor configuration which is incompatible with the robot (for example, LIDAR configuration)."""
[docs]class AreaCallbackMapError(GraphNavServiceResponseError): """The map specified an area callback that is not registered or is faulted."""
[docs]class RequestAbortedError(GraphNavServiceResponseError): """Request was aborted by the system."""
[docs]class RequestFailedError(GraphNavServiceResponseError): """Request failed to complete by the system."""
[docs]class RobotFaultedError(GraphNavServiceResponseError): """Robot is experiencing a fault condition that prevents localization."""
[docs]class UnknownMapInformationError(GraphNavServiceResponseError): """The given map information (waypoints,edges,routes) is unknown by the system."""
[docs]class TimeError(GraphNavServiceResponseError): """Errors associated with timestamps and time sync."""
[docs]class CommandExpiredError(TimeError): """The command was received after its end time had already passed."""
[docs]class NoTimeSyncError(TimeError): """Client has not performed timesync with robot."""
[docs]class TooDistantError(TimeError): """The command was too far in the future."""
[docs]class RobotStateError(GraphNavServiceResponseError): """Errors associated with the current state of the robot."""
[docs]class IsRecordingError(RobotStateError): """Cannot navigate a route while recording a map."""
[docs]class CannotModifyMapDuringRecordingError(RobotStateError): """Cannot clear the map during recording. Call StopRecording first."""
[docs]class RobotImpairedError(RobotStateError): """Robot has a critical perception or behavior fault and cannot navigate."""
[docs]class RouteError(GraphNavServiceResponseError): """Errors associated with the specified route."""
[docs]class ConstraintFaultError(RouteError): """Route parameters contained a constraint fault."""
[docs]class InvalidEdgeError(RouteError): """One or more edges do not connect to expected waypoints."""
[docs]@deprecated(reason='Use UnknownRouteElementsError instead', version='3.0.0', action='ignore') class UnkownRouteElementsError(RouteError): """One or more waypoints/edges are not in the map."""
[docs]class UnknownRouteElementsError(UnkownRouteElementsError): """One or more waypoints/edges are not in the map."""
[docs]class NoPathError(RouteError): """There is no path to the specified waypoint."""
[docs]class UnknownWaypointError(RouteError): """One or more waypoints are not in the map."""
[docs]class NoAnchoringError(RouteError): """There is no anchoring."""
[docs]class InvalidPoseError(RouteError): """The requested pose is invalid, or known to be unachievable."""
[docs]class RouteNavigationError(GraphNavServiceResponseError): """Errors related to how the robot navigates the route."""
[docs]class FeatureDesertError(RouteNavigationError): """Route contained too many waypoints with low-quality features."""
[docs]class RouteNotUpdatingError(RouteNavigationError): """Graph nav was unable to update and follow the specified route."""
[docs]class RobotLostError(RouteNavigationError): """Cannot issue a navigation request when the robot is already lost."""
[docs]class InvalidGPSError(RouteNavigationError): """Cannot issue the GPS command because it is invalid.""" def _gps_status_to_string(self, status): if status == graph_nav_pb2.NavigateToAnchorResponse.GPS_STATUS_OK: return 'OK' elif status == graph_nav_pb2.NavigateToAnchorResponse.GPS_STATUS_NO_COORDS_IN_MAP: return 'The uploaded map did not contain any valid GPS coordinates.' elif status == graph_nav_pb2.NavigateToAnchorResponse.GPS_STATUS_TOO_FAR_FROM_MAP: return 'The given coordinates were too far from any coordinates in the uploaded map.' else: return 'Unknown error' def __str__(self): return f'{self.error_message} (reason: {self._gps_status_to_string(self.response.gps_status)})'
[docs]class RobotNotLocalizedToRouteError(RouteNavigationError): """The current localization doesn't refer to any waypoint in the route (possibly uninitialized localization)."""
[docs]class RobotStuckError(RouteNavigationError): """The robot is stuck or unable to find a way forward. Resend the command with a new ID, or send a different command to try again."""
[docs]@deprecated(reason='Use UnrecognizedCommandError instead', version='3.1.0', action='ignore') class UnrecongizedCommandError(RouteNavigationError): """Happens when you try to continue a command that was either expired, or had an unrecognized id."""
[docs]class UnrecognizedCommandError(UnrecongizedCommandError): """Happens when you try to continue a command that was either expired, or had an unrecognized id."""
def _localization_from_response(response): """Return the localization state from the response.""" return response.localization def _command_id_from_navigate_route_response(response): """Return the navigation command id from the response.""" return response.command_id def _get_status(response): """Return the status of the response.""" return response.status def _get_response(response): """Return full response for RecordStatus to get environment and is_recording information.""" return response def _get_graph(response): """Returns the graph from the response.""" return response.graph def _get_streamed_data(response, data_type): """Given a list of streamed responses, return an instance of the given data type that is parsed from those responses.""" data = bytes() for resp in response: data += resp.chunk.data proto_instance = data_type() proto_instance.ParseFromString(data) return proto_instance def _get_streamed_download_graph(response): """Reads a streamed response to recreate a DownloadGraphRequest""" download_graph = _get_streamed_data(response, graph_nav_pb2.DownloadGraphResponse) return download_graph.graph def _get_streamed_waypoint_snapshot(response): """Reads a streamed response to recreate a waypoint snapshot.""" return _get_streamed_data(response, map_pb2.WaypointSnapshot) def _get_streamed_edge_snapshot(response): """Reads a streamed response to recreate an edge snapshot.""" return _get_streamed_data(response, map_pb2.EdgeSnapshot) _UPLOAD_GRAPH_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _UPLOAD_GRAPH_STATUS_TO_ERROR.update({ graph_nav_pb2.UploadGraphResponse.STATUS_OK: (None, None), graph_nav_pb2.UploadGraphResponse.STATUS_MAP_TOO_LARGE_LICENSE: error_pair(MapTooLargeLicenseError), graph_nav_pb2.UploadGraphResponse.STATUS_INVALID_GRAPH: error_pair(InvalidGraphError), graph_nav_pb2.UploadGraphResponse.STATUS_INCOMPATIBLE_SENSORS: error_pair(IncompatibleSensorsError), graph_nav_pb2.UploadGraphResponse.STATUS_AREA_CALLBACK_ERROR: error_pair(AreaCallbackMapError), }) @handle_common_header_errors @handle_lease_use_result_errors @handle_license_errors_if_present @handle_unset_status_error(unset='STATUS_UNKNOWN') def _upload_graph_error(response): """Return a custom exception based on upload graph response, None if no error.""" return error_factory(response, response.status, status_to_string=graph_nav_pb2.UploadGraphResponse.Status.Name, status_to_error=_UPLOAD_GRAPH_STATUS_TO_ERROR) _UPLOAD_WAYPOINT_SNAPSHOT_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _UPLOAD_WAYPOINT_SNAPSHOT_TO_ERROR.update({ graph_nav_pb2.UploadWaypointSnapshotResponse.STATUS_UNKNOWN: (None, None), graph_nav_pb2.UploadWaypointSnapshotResponse.STATUS_OK: (None, None), graph_nav_pb2.UploadWaypointSnapshotResponse.STATUS_INCOMPATIBLE_SENSORS: error_pair(IncompatibleSensorsError) }) _CLEAR_GRAPH_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _CLEAR_GRAPH_STATUS_TO_ERROR.update({ # Unknown should not produce an error for backwards compatibility purposes (introduced in 3.1). graph_nav_pb2.ClearGraphResponse.STATUS_UNKNOWN: (None, None), graph_nav_pb2.ClearGraphResponse.STATUS_OK: (None, None), graph_nav_pb2.ClearGraphResponse.STATUS_RECORDING: error_pair(CannotModifyMapDuringRecordingError), }) @handle_common_header_errors @handle_lease_use_result_errors def _clear_graph_error(response): """Return a custom exception based on upload graph response, None if no error.""" return error_factory(response, response.status, status_to_string=graph_nav_pb2.ClearGraphResponse.Status.Name, status_to_error=_CLEAR_GRAPH_STATUS_TO_ERROR) @handle_common_header_errors @handle_lease_use_result_errors def _upload_waypoint_snapshot_error(response): """Return a custom exception based on upload graph response, None if no error.""" return error_factory(response, response.status, status_to_string=graph_nav_pb2.UploadWaypointSnapshotResponse.Status.Name, status_to_error=_UPLOAD_WAYPOINT_SNAPSHOT_TO_ERROR) _SET_LOCALIZATION_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _SET_LOCALIZATION_STATUS_TO_ERROR.update({ graph_nav_pb2.SetLocalizationResponse.STATUS_OK: (None, None), graph_nav_pb2.SetLocalizationResponse.STATUS_ROBOT_IMPAIRED: error_pair(RobotFaultedError), graph_nav_pb2.SetLocalizationResponse.STATUS_UNKNOWN_WAYPOINT: (UnknownMapInformationError, UnknownMapInformationError.__doc__ + " The waypoint is unknown."), graph_nav_pb2.SetLocalizationResponse.STATUS_ABORTED: error_pair(RequestAbortedError), graph_nav_pb2.SetLocalizationResponse.STATUS_FAILED: error_pair(RequestFailedError), graph_nav_pb2.SetLocalizationResponse.STATUS_INCOMPATIBLE_SENSORS: error_pair(IncompatibleSensorsError) }) @handle_common_header_errors @handle_lease_use_result_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _set_localization_error(response): """Return a custom exception based on set localization response, None if no error.""" return error_factory(response, response.status, status_to_string=graph_nav_pb2.SetLocalizationResponse.Status.Name, status_to_error=_SET_LOCALIZATION_STATUS_TO_ERROR) _NAVIGATE_ROUTE_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _NAVIGATE_ROUTE_STATUS_TO_ERROR.update({ graph_nav_pb2.NavigateRouteResponse.STATUS_OK: (None, None), graph_nav_pb2.NavigateRouteResponse.STATUS_NO_TIMESYNC: error_pair(NoTimeSyncError), graph_nav_pb2.NavigateRouteResponse.STATUS_EXPIRED: error_pair(CommandExpiredError), graph_nav_pb2.NavigateRouteResponse.STATUS_TOO_DISTANT: error_pair(TooDistantError), graph_nav_pb2.NavigateRouteResponse.STATUS_ROBOT_IMPAIRED: error_pair(RobotImpairedError), graph_nav_pb2.NavigateRouteResponse.STATUS_RECORDING: error_pair(IsRecordingError), graph_nav_pb2.NavigateRouteResponse.STATUS_UNKNOWN_ROUTE_ELEMENTS: error_pair(UnknownRouteElementsError), graph_nav_pb2.NavigateRouteResponse.STATUS_INVALID_EDGE: error_pair(InvalidEdgeError), graph_nav_pb2.NavigateRouteResponse.STATUS_NO_PATH: error_pair(NoPathError), graph_nav_pb2.NavigateRouteResponse.STATUS_CONSTRAINT_FAULT: error_pair(ConstraintFaultError), graph_nav_pb2.NavigateRouteResponse.STATUS_FEATURE_DESERT: error_pair(FeatureDesertError), graph_nav_pb2.NavigateRouteResponse.STATUS_LOST: error_pair(RobotLostError), graph_nav_pb2.NavigateRouteResponse.STATUS_NOT_LOCALIZED_TO_ROUTE: error_pair(RobotNotLocalizedToRouteError), graph_nav_pb2.NavigateRouteResponse.STATUS_NOT_LOCALIZED_TO_MAP: error_pair(RobotNotLocalizedToRouteError), graph_nav_pb2.NavigateRouteResponse.STATUS_COULD_NOT_UPDATE_ROUTE: error_pair(RouteNotUpdatingError), graph_nav_pb2.NavigateRouteResponse.STATUS_STUCK: error_pair(RobotStuckError), graph_nav_pb2.NavigateRouteResponse.STATUS_UNRECOGNIZED_COMMAND: error_pair(UnrecognizedCommandError), graph_nav_pb2.NavigateRouteResponse.STATUS_AREA_CALLBACK_ERROR: error_pair(AreaCallbackMapError), }) @handle_common_header_errors @handle_lease_use_result_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _navigate_route_error(response): """Return a custom exception based on navigate route response, None if no error.""" return error_factory(response, response.status, status_to_string=graph_nav_pb2.NavigateRouteResponse.Status.Name, status_to_error=_NAVIGATE_ROUTE_STATUS_TO_ERROR) _NAVIGATE_TO_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _NAVIGATE_TO_STATUS_TO_ERROR.update({ graph_nav_pb2.NavigateToResponse.STATUS_OK: (None, None), graph_nav_pb2.NavigateToResponse.STATUS_NO_TIMESYNC: error_pair(NoTimeSyncError), graph_nav_pb2.NavigateToResponse.STATUS_EXPIRED: error_pair(CommandExpiredError), graph_nav_pb2.NavigateToResponse.STATUS_TOO_DISTANT: error_pair(TooDistantError), graph_nav_pb2.NavigateToResponse.STATUS_ROBOT_IMPAIRED: error_pair(RobotImpairedError), graph_nav_pb2.NavigateToResponse.STATUS_RECORDING: error_pair(IsRecordingError), graph_nav_pb2.NavigateToResponse.STATUS_NO_PATH: error_pair(NoPathError), graph_nav_pb2.NavigateToResponse.STATUS_UNKNOWN_WAYPOINT: error_pair(UnknownWaypointError), graph_nav_pb2.NavigateToResponse.STATUS_FEATURE_DESERT: error_pair(FeatureDesertError), graph_nav_pb2.NavigateToResponse.STATUS_LOST: error_pair(RobotLostError), graph_nav_pb2.NavigateToResponse.STATUS_NOT_LOCALIZED_TO_MAP: error_pair(RobotNotLocalizedToRouteError), graph_nav_pb2.NavigateToResponse.STATUS_COULD_NOT_UPDATE_ROUTE: error_pair(RouteNotUpdatingError), graph_nav_pb2.NavigateToResponse.STATUS_STUCK: error_pair(RobotStuckError), graph_nav_pb2.NavigateToResponse.STATUS_UNRECOGNIZED_COMMAND: error_pair(UnrecognizedCommandError), graph_nav_pb2.NavigateToResponse.STATUS_AREA_CALLBACK_ERROR: error_pair(AreaCallbackMapError), }) @handle_common_header_errors @handle_lease_use_result_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _navigate_to_error(response): """Return a custom exception based on navigate to response, None if no error.""" return error_factory(response, response.status, status_to_string=graph_nav_pb2.NavigateToResponse.Status.Name, status_to_error=_NAVIGATE_TO_STATUS_TO_ERROR) _NAVIGATE_TO_ANCHOR_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _NAVIGATE_TO_ANCHOR_STATUS_TO_ERROR.update({ graph_nav_pb2.NavigateToAnchorResponse.STATUS_OK: (None, None), graph_nav_pb2.NavigateToAnchorResponse.STATUS_NO_TIMESYNC: error_pair(NoTimeSyncError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_EXPIRED: error_pair(CommandExpiredError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_TOO_DISTANT: error_pair(TooDistantError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_ROBOT_IMPAIRED: error_pair(RobotImpairedError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_RECORDING: error_pair(IsRecordingError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_NO_PATH: error_pair(NoPathError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_NO_ANCHORING: error_pair(NoAnchoringError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_FEATURE_DESERT: error_pair(FeatureDesertError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_LOST: error_pair(RobotLostError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_NOT_LOCALIZED_TO_MAP: error_pair(RobotNotLocalizedToRouteError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_COULD_NOT_UPDATE_ROUTE: error_pair(RouteNotUpdatingError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_STUCK: error_pair(RobotStuckError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_INVALID_POSE: error_pair(InvalidPoseError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_UNRECOGNIZED_COMMAND: error_pair(UnrecognizedCommandError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_AREA_CALLBACK_ERROR: error_pair(AreaCallbackMapError), graph_nav_pb2.NavigateToAnchorResponse.STATUS_INVALID_GPS_COMMAND: error_pair(InvalidGPSError) }) @handle_common_header_errors @handle_lease_use_result_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _navigate_to_anchor_error(response): """Return a custom exception based on navigate to anchor response, None if no error.""" return error_factory(response, response.status, status_to_string=graph_nav_pb2.NavigateToAnchorResponse.Status.Name, status_to_error=_NAVIGATE_TO_ANCHOR_STATUS_TO_ERROR) @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _navigate_feedback_error(response): """Return a custom exception based on navigate to response, None if no error.""" # If the common response header is OK and the status is set, no error. return None @handle_common_header_errors def _download_graph_stream_errors(response): """Return a custom exception based on download graph streaming response, None if no error.""" return None @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _download_waypoint_snapshot_stream_errors(response): """Return a custom exception based on download waypoint snapshot streaming response, None if no error.""" # Iterate through the response since the download request responds with a stream. for resp in response: # Handle error statuses from the request. if (resp.status == graph_nav_pb2.DownloadWaypointSnapshotResponse.STATUS_SNAPSHOT_DOES_NOT_EXIST): return UnknownMapInformationError(response=resp, error_message=UnknownMapInformationError.__doc__) # All responses (in the iterator) had status_ok return None @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _download_edge_snapshot_stream_errors(response): """Return a custom exception based on download edge snapshot streaming response, None if no error.""" # Iterate through the response since the download request responds with a stream. for resp in response: # Handle error statuses from the request. if (resp.status == graph_nav_pb2.DownloadEdgeSnapshotResponse.STATUS_SNAPSHOT_DOES_NOT_EXIST ): return UnknownMapInformationError(response=resp, error_message=UnknownMapInformationError.__doc__) # All responses (in the iterator) had status_ok return None