Source code for bosdyn.client.hazard_avoidance

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""For clients to use the hazard_avoidance service."""

import collections

from bosdyn.api import hazard_avoidance_pb2
from bosdyn.api import hazard_avoidance_service_pb2_grpc as hazard_avoidance_service
from bosdyn.client.common import (
    BaseClient,
    custom_params_error,
    error_factory,
    error_pair,
    handle_common_header_errors,
)
from bosdyn.client.exceptions import InvalidRequestError, ResponseError, UnsetStatusError
from bosdyn.client.robot_command import NoTimeSyncError
from bosdyn.client.time_sync import update_timestamp_filter


[docs]class AddHazardsResponseError(ResponseError): """General class of errors for hazard avoidance service."""
_ADD_HAZARD_STATUS_TO_ERROR = collections.defaultdict(lambda: (AddHazardsResponseError, None)) _ADD_HAZARD_STATUS_TO_ERROR.update({ hazard_avoidance_pb2.AddHazardResult.STATUS_HAZARDS_UPDATED: (None, None), hazard_avoidance_pb2.AddHazardResult.STATUS_IGNORED: (None, None), hazard_avoidance_pb2.AddHazardResult.STATUS_INVALID_DATA: error_pair(InvalidRequestError), hazard_avoidance_pb2.AddHazardResult.STATUS_UNKNOWN: error_pair(UnsetStatusError), }) @handle_common_header_errors def _error_from_response(response): """Return a custom exception based on the first invalid add hazard result, None if no error.""" for add_hazard_result in response.add_hazard_results: result = custom_params_error(add_hazard_result, total_response=response) if result is not None: return result result = error_factory(response, add_hazard_result.status, status_to_string=hazard_avoidance_pb2.AddHazardResult.Status.Name, status_to_error=_ADD_HAZARD_STATUS_TO_ERROR) if result is not None: # The exception is using the add hazards result. Replace it with the full response. result.response = response return result return None def _get_add_hazards_value(response): return response.add_hazard_results
[docs]class HazardAvoidanceClient(BaseClient): """Client for Hazard avoidance service.""" default_service_name = 'hazard-avoidance-service' service_type = 'bosdyn.api.HazardAvoidanceService' def __init__(self): super(HazardAvoidanceClient, self).__init__(hazard_avoidance_service.HazardAvoidanceServiceStub) self._timesync_endpoint = None
[docs] def update_from(self, other): super(HazardAvoidanceClient, self).update_from(other) # Grab a timesync endpoint if it is available. try: self._timesync_endpoint = other.time_sync.endpoint except AttributeError: pass # other doesn't have a time_sync accessor
@property def timesync_endpoint(self): """Accessor for timesync-endpoint that is grabbed via 'update_from()'. Raises: bosdyn.client.robot_command.NoTimeSyncError: Could not find the timesync endpoint for the robot. """ if not self._timesync_endpoint: raise NoTimeSyncError("[world object service] No timesync endpoint set for the robot") return self._timesync_endpoint
[docs] def add_hazards(self, add_hazards_req, **kwargs): """Add hazards to the hazard map. Args: add_hazards_req (hazard_avoidance_pb2.AddHazardsRequest): The request including the hazard observations to add. Returns: response (hazard_avoidance_pb2.AddHazardsResponse): Contains the status of adding each observation, Raises: RpcError: Problem communicating with the robot. bosdyn.client.robot_command.NoTimeSyncError: Couldn't convert the timestamp into robot time. UnsetStatusError: An internal HazardAvoidanceService issue has happened. AddHazardsResponseError: General problem with the request. bosdyn.client.exceptions.InvalidRequestError: One or more hazard observations contained errors. """ for hazard_obs in add_hazards_req.hazards: if hazard_obs.HasField("acquisition_time"): # Ensure the hazard observation's time of detection is in robot time. client_timestamp = hazard_obs.acquisition_time hazard_obs.acquisition_time.CopyFrom( update_timestamp_filter(self, client_timestamp, self.timesync_endpoint)) return self.call(self._stub.AddHazards, add_hazards_req, _get_add_hazards_value, _error_from_response, copy_request=False, **kwargs)
[docs] def add_hazards_async(self, add_hazards_req, **kwargs): """Async version of add_hazards().""" for hazard_obs in add_hazards_req.hazards: if hazard_obs.HasField("acquisition_time"): # Ensure the hazard observation's time of detection is in robot time. client_timestamp = hazard_obs.acquisition_time hazard_obs.acquisition_time.CopyFrom( update_timestamp_filter(self, client_timestamp, self.timesync_endpoint)) return self.call_async(self._stub.AddHazards, add_hazards_req, _get_add_hazards_value, _error_from_response, copy_request=False, **kwargs)