Source code for bosdyn.client.map_processing

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""For clients of the graph_nav map processing service."""

from bosdyn.api.graph_nav import map_pb2, map_processing_pb2, map_processing_service_pb2
from bosdyn.api.graph_nav import map_processing_service_pb2_grpc as map_processing
from bosdyn.client.common import (BaseClient, common_header_errors, error_factory,
                                  handle_common_header_errors, handle_lease_use_result_errors,
                                  handle_unset_status_error)
from bosdyn.client.exceptions import ResponseError


[docs]class MapProcessingServiceResponseError(ResponseError): """General class of errors for the GraphNav map processing service."""
[docs]class MissingSnapshotsError(MapProcessingServiceResponseError): """The uploaded map has missing waypoint snapshots."""
[docs]class OptimizationFailureError(MapProcessingServiceResponseError): """The anchoring optimization failed."""
[docs]class InvalidGraphError(MapProcessingServiceResponseError): """The graph is invalid topologically, for example containing missing waypoints referenced by edges."""
[docs]class InvalidParamsError(MapProcessingServiceResponseError): """The parameters passed to the optimizer do not make sense (e.g. negative weights)."""
[docs]class MaxIterationsError(MapProcessingServiceResponseError): """The optimizer reached the maximum number of iterations before converging."""
[docs]class MaxTimeError(MapProcessingServiceResponseError): """The optimizer timed out before converging."""
[docs]class InvalidHintsError(MapProcessingServiceResponseError): """One or more of the hints passed in to the optimizer are invalid (do not correspond to real waypoints or objects)."""
[docs]class InvalidGravityAlignmentError(MapProcessingServiceResponseError): """One or more anchoring hints disagrees with gravity. Ensure the orientation of any hints is correct."""
[docs]class ConstraintViolationError(MapProcessingServiceResponseError): """One or more anchors were moved outside of the desired constraints."""
[docs]class MapModifiedError(MapProcessingServiceResponseError): """The map was modified on the server by another client during processing. Please try again."""
@handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _process_topology_common_errors(response): # Handle error statuses from the request. if (response.status == map_processing_pb2.ProcessTopologyResponse.STATUS_INVALID_GRAPH): return InvalidGraphError(response=response, error_message=InvalidGraphError.__doc__) elif (response.status == map_processing_pb2.ProcessTopologyResponse.STATUS_MISSING_WAYPOINT_SNAPSHOTS): return MissingSnapshotsError(response=response, error_message=MissingSnapshotsError.__doc__) elif (response.status == map_processing_pb2.ProcessTopologyResponse.STATUS_MAP_MODIFIED_DURING_PROCESSING): return MapModifiedError(response=response, error_message=MapModifiedError.__doc__) return None def _process_topology_streamed_errors(responses): """Return a custom exception based on process topology streaming response, None if no error.""" # Iterate through the response since the request responds with a stream. for resp in responses: exception = _process_topology_common_errors(resp) if exception: return exception # All responses (in the iterator) had status_ok return None __ANCHORING_COMMON_ERRORS = { map_processing_pb2.ProcessAnchoringResponse.STATUS_MISSING_WAYPOINT_SNAPSHOTS: MissingSnapshotsError, map_processing_pb2.ProcessAnchoringResponse.STATUS_OPTIMIZATION_FAILURE: OptimizationFailureError, map_processing_pb2.ProcessAnchoringResponse.STATUS_INVALID_GRAPH: InvalidGraphError, map_processing_pb2.ProcessAnchoringResponse.STATUS_INVALID_PARAMS: InvalidParamsError, map_processing_pb2.ProcessAnchoringResponse.STATUS_CONSTRAINT_VIOLATION: ConstraintViolationError, map_processing_pb2.ProcessAnchoringResponse.STATUS_MAX_ITERATIONS: MaxIterationsError, map_processing_pb2.ProcessAnchoringResponse.STATUS_MAX_TIME: MaxTimeError, map_processing_pb2.ProcessAnchoringResponse.STATUS_INVALID_HINTS: InvalidHintsError, map_processing_pb2.ProcessAnchoringResponse.STATUS_INVALID_GRAVITY_ALIGNMENT: InvalidGravityAlignmentError, map_processing_pb2.ProcessAnchoringResponse.STATUS_MAP_MODIFIED_DURING_PROCESSING: MapModifiedError } @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _process_anchoring_common_errors(response): # Handle error statuses from the request. if response.status in __ANCHORING_COMMON_ERRORS: type_name = __ANCHORING_COMMON_ERRORS[response.status] return type_name(response=response, error_message=type_name.__doc__) return None def _process_anchoring_streamed_errors(responses): """Return a custom exception based on process anchoring streaming response, None if no error.""" # Iterate through the response since the request responds with a stream. for resp in responses: exception = _process_anchoring_common_errors(resp) if exception: return exception # All responses (in the iterator) had status_ok return None def _get_streamed_topology_response(response): """Reads a streamed response to recreate a merged topology response.""" merged_response = map_processing_pb2.ProcessTopologyResponse() for resp in response: merged_response.MergeFrom(resp) return merged_response def _get_streamed_anchoring_response(response): """Reads a streamed response to recreate a merged anchoring response.""" merged_response = map_processing_pb2.ProcessAnchoringResponse() for resp in response: merged_response.MergeFrom(resp) return merged_response
[docs]class MapProcessingServiceClient(BaseClient): """Client for the GraphNav map processing service.""" default_service_name = 'map-processing-service' service_type = 'bosdyn.api.graph_nav.MapProcessingService' def __init__(self): super(MapProcessingServiceClient, self).__init__(map_processing.MapProcessingServiceStub) @staticmethod def _build_process_topology_request(params, modify_map_on_server): return map_processing_pb2.ProcessTopologyRequest(params=params, modify_map_on_server=modify_map_on_server) @staticmethod def _build_process_anchoring_request(params, modify_anchoring_on_server, stream_intermediate_results, initial_hint, apply_gps_results): return map_processing_pb2.ProcessAnchoringRequest( params=params, initial_hint=initial_hint, modify_anchoring_on_server=modify_anchoring_on_server, stream_intermediate_results=stream_intermediate_results, apply_gps_result_to_waypoints_on_server=apply_gps_results)
[docs] def process_topology(self, params, modify_map_on_server, **kwargs): """Process the topology of the map on the server, closing loops and producing a consistent topology. Args: params: a ProcessTopologyRequest.Params object modify_map_on_server: if true, the map will be modified on the server. If false, the subgraph returned by this function should be uploaded back to the server if it is to be reused. Returns: The ProcessTopologyResponse containing new edges to add to the map. Raises: RpcError: Problem communicating with the robot """ request = self._build_process_topology_request(params, modify_map_on_server) return self.call(self._stub.ProcessTopology, request, value_from_response=_get_streamed_topology_response, error_from_response=_process_topology_streamed_errors, copy_request=False, **kwargs)
[docs] def process_anchoring(self, params, modify_anchoring_on_server, stream_intermediate_results, initial_hint=None, apply_gps_results=False, **kwargs): """Process the anchoring of the map on the server, producing a metrically consistent anchoring. Args: params: a ProcessAnchoringRequest.Params object modify_anchoring_on_server: if true, the map will be modified on the server. If false, the anchoring returned by this function should be uploaded back to the server if it is to be reused. stream_intermediate_results: if true, anchorings from earlier optimizer iterations may be included in the response. If false, only the last iteration will be returned. initial_hint: Initial guess at some number of waypoints and world objects and their anchorings. This field is an AnchoringHint object (see map_processing.proto) apply_gps_results: if true, the annotations of waypoints in the graph will be modified to include the pose of each waypoint in a GPS centered frame, if the map has GPS (see map_processing.proto) Returns: The ProcessAnchoringResponse containing a new optimized anchoring. Raises: RpcError: Problem communicating with the robot """ request = self._build_process_anchoring_request(params, modify_anchoring_on_server, stream_intermediate_results, initial_hint, apply_gps_results) return self.call(self._stub.ProcessAnchoring, request, value_from_response=_get_streamed_anchoring_response, error_from_response=_process_anchoring_streamed_errors, copy_request=False, **kwargs)