Source code for bosdyn.client.spot_cam.power

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""For clients to the Spot CAM Power service."""

import logging

_LOGGER = logging.getLogger(__name__)

from google.protobuf.wrappers_pb2 import BoolValue

from bosdyn.api.spot_cam import power_pb2, service_pb2_grpc
from bosdyn.client.common import BaseClient, handle_common_header_errors


[docs]class PowerClient(BaseClient): """A client calling Spot CAM Power service.""" default_service_name = 'spot-cam-power' service_type = 'bosdyn.api.spot_cam.PowerService' def __init__(self): super(PowerClient, self).__init__(service_pb2_grpc.PowerServiceStub)
[docs] def get_power_status(self, **kwargs): """Retrieve on/off state of device.""" request = power_pb2.GetPowerStatusRequest() return self.call(self._stub.GetPowerStatus, request, self._get_power_status_from_response, self._power_error_from_response, copy_request=False, **kwargs)
[docs] def get_power_status_async(self, **kwargs): """Async version of get_power_status()""" request = power_pb2.GetPowerStatusRequest() return self.call_async(self._stub.GetPowerStatus, request, self._get_power_status_from_response, self._power_error_from_response, copy_request=False, **kwargs)
[docs] def set_power_status(self, ptz=None, aux1=None, aux2=None, external_mic=None, **kwargs): """Turn on/off the desire device. Should not be used on PTZ for non-IR units as it can cause the stream to crash. If the intent is to reset the PTZ autofocus, try PtzClient.initialize_lens instead. If the intent is to recover the PTZ stream in another way, you may need to power cycle the robot. """ request = self._build_SetPowerStatusRequest(ptz, aux1, aux2, external_mic) return self.call(self._stub.SetPowerStatus, request, self._set_power_status_from_response, self._power_error_from_response, copy_request=False, **kwargs)
[docs] def set_power_status_async(self, ptz=None, aux1=None, aux2=None, external_mic=None, **kwargs): """Async version of set_power_status()""" request = self._build_SetPowerStatusRequest(ptz, aux1, aux2, external_mic) return self.call_async(self._stub.SetPowerStatus, request, self._set_power_status_from_response, self._power_error_from_response, copy_request=False, **kwargs)
[docs] def cycle_power(self, ptz=None, aux1=None, aux2=None, external_mic=None, **kwargs): """Turn power off then back on for the desired devices. Should not be used on PTZ for non-IR units as it can cause the stream to crash. If the intent is to reset the PTZ autofocus, try PtzClient.initialize_lens instead. If the intent is to recover the PTZ stream in another way, you may need to power cycle the robot. """ request = self._build_CyclePowerRequest(ptz, aux1, aux2, external_mic) return self.call(self._stub.CyclePower, request, self._cycle_power_from_response, self._power_error_from_response, copy_request=False, **kwargs)
[docs] def cycle_power_async(self, ptz=None, aux1=None, aux2=None, external_mic=None, **kwargs): """Async version of cycle_power()""" request = self._build_CyclePowerRequest(ptz, aux1, aux2, external_mic) return self.call_async(self._stub.CyclePower, request, self._cycle_power_from_response, self._power_error_from_response, copy_request=False, **kwargs)
@staticmethod def _build_SetPowerStatusRequest(ptz, aux1, aux2, external_mic): request = power_pb2.SetPowerStatusRequest() if ptz: request.status.ptz.value = ptz if aux1: request.status.aux1.value = aux1 if aux2: request.status.aux2.value = aux2 if external_mic: request.status.external_mic.value = external_mic return request @staticmethod def _build_CyclePowerRequest(ptz, aux1, aux2, external_mic): request = power_pb2.CyclePowerRequest() if ptz: request.status.ptz.value = ptz if aux1: request.status.aux1.value = aux1 if aux2: request.status.aux2.value = aux2 if external_mic: request.status.external_mic.value = external_mic return request @staticmethod def _get_power_status_from_response(response): return response.status @staticmethod def _set_power_status_from_response(response): return response.status @staticmethod def _cycle_power_from_response(response): return response.status @staticmethod @handle_common_header_errors def _power_error_from_response(response): # pylint: disable=unused-argument return None