Source code for bosdyn.client.spot_cam.ptz

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""For clients to the Spot CAM Ptz service."""

import logging

_LOGGER = logging.getLogger(__name__)

from google.protobuf.wrappers_pb2 import FloatValue, Int32Value

from bosdyn.api.spot_cam import ptz_pb2, service_pb2_grpc
from bosdyn.client.common import BaseClient, common_header_errors, handle_common_header_errors
from bosdyn.client.math_helpers import recenter_value_mod


[docs]class PtzClient(BaseClient): """A client calling Spot CAM Ptz service. """ default_service_name = 'spot-cam-ptz' service_type = 'bosdyn.api.spot_cam.PtzService' def __init__(self): super(PtzClient, self).__init__(service_pb2_grpc.PtzServiceStub)
[docs] def list_ptz(self, **kwargs): """List all the available ptzs""" request = ptz_pb2.ListPtzRequest() return self.call(self._stub.ListPtz, request, self._list_ptz_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def list_ptz_async(self, **kwargs): """Async version of list_ptz()""" request = ptz_pb2.ListPtzRequest() return self.call_async(self._stub.ListPtz, request, self._list_ptz_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def get_ptz_position(self, ptz_desc, **kwargs): """Position of the specified ptz""" request = ptz_pb2.GetPtzPositionRequest(ptz=ptz_desc) return self.call(self._stub.GetPtzPosition, request, self._get_ptz_position_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def get_ptz_position_async(self, ptz_desc, **kwargs): """Async version of get_ptz_position()""" request = ptz_pb2.GetPtzPositionRequest(ptz=ptz_desc) return self.call_async(self._stub.GetPtzPosition, request, self._get_ptz_position_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def get_ptz_velocity(self, ptz_desc, **kwargs): """Velocity of the specified ptz""" request = ptz_pb2.GetPtzVelocityRequest(ptz=ptz_desc) return self.call(self._stub.GetPtzVelocity, request, self._get_ptz_velocity_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def get_ptz_velocity_async(self, ptz_desc, **kwargs): """Async version of get_ptz_velocity()""" request = ptz_pb2.GetPtzVelocityRequest(ptz=ptz_desc) return self.call_async(self._stub.GetPtzVelocity, request, self._get_ptz_velocity_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def set_ptz_position(self, ptz_desc, pan, tilt, zoom, **kwargs): """Set position of the specified ptz in PTZ-space""" p = FloatValue(value=pan) t = FloatValue(value=tilt) z = FloatValue(value=zoom) ptz_position = ptz_pb2.PtzPosition(ptz=ptz_desc, pan=p, tilt=t, zoom=z) request = ptz_pb2.SetPtzPositionRequest(position=ptz_position) return self.call(self._stub.SetPtzPosition, request, self._set_ptz_position_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def set_ptz_position_async(self, ptz_desc, pan, tilt, zoom, **kwargs): """Async version of set_ptz_position()""" p = FloatValue(value=pan) t = FloatValue(value=tilt) z = FloatValue(value=zoom) ptz_position = ptz_pb2.PtzPosition(ptz=ptz_desc, pan=p, tilt=t, zoom=z) request = ptz_pb2.SetPtzPositionRequest(position=ptz_position) return self.call_async(self._stub.SetPtzPosition, request, self._set_ptz_position_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def set_ptz_velocity(self, ptz_desc, pan, tilt, zoom, **kwargs): """Set velocity of the specified ptz in PTZ-space""" p = FloatValue(value=pan) t = FloatValue(value=tilt) z = FloatValue(value=zoom) ptz_velocity = ptz_pb2.PtzVelocity(ptz=ptz_desc, pan=p, tilt=t, zoom=z) request = ptz_pb2.SetPtzVelocityRequest(velocity=ptz_velocity) return self.call(self._stub.SetPtzVelocity, request, self._set_ptz_velocity_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def set_ptz_velocity_async(self, ptz_desc, pan, tilt, zoom, **kwargs): """Async version of set_ptz_velocity()""" p = FloatValue(value=pan) t = FloatValue(value=tilt) z = FloatValue(value=zoom) ptz_velocity = ptz_pb2.PtzVelocity(ptz=ptz_desc, pan=p, tilt=t, zoom=z) request = ptz_pb2.SetPtzVelocityRequest(velocity=ptz_velocity) return self.call_async(self._stub.SetPtzVelocity, request, self._set_ptz_velocity_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def initialize_lens(self, **kwargs): """Initializes the PTZ autofocus or resets it if already initialized""" request = ptz_pb2.InitializeLensRequest() return self.call(self._stub.InitializeLens, request, self._initialize_lens_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def initialize_lens_async(self, **kwargs): """Async version of initialize_lens()""" request = ptz_pb2.InitializeLensRequest() return self.call_async(self._stub.InitializeLens, request, self._initialize_lens_from_response, common_header_errors, copy_request=False, **kwargs)
# Manual Focus RPCs
[docs] def get_ptz_focus_state(self, **kwargs): """Retrieve focus of the mechanical ptz Args: focus_mode (PtzFocusMode): Enum indicating whether to autofocus or manually focus distance (float): Approximate distance to focus on, most accurate between 1.2m and 20m, only settable in PTZ_FOCUS_MANUAL mode focus_position (int32): Precise lens position for the camera for repeatable operations, overrides distance if specified, only settable in PTZ_FOCUS_MANUAL mode Returns: PtzFocusState containing the current focus mode and position """ request = ptz_pb2.GetPtzFocusStateRequest() return self.call(self._stub.GetPtzFocusState, request, self._get_ptz_focus_state_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def get_ptz_focus_state_async(self, **kwargs): """Async version of get_ptz_focus_state()""" request = ptz_pb2.GetPtzFocusStateRequest() return self.call_async(self._stub.GetPtzFocusState, request, self._get_ptz_focus_state_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def set_ptz_focus_state(self, focus_mode, distance=None, focus_position=None, **kwargs): """Set focus of the mechanical ptz Args: focus_mode (PtzFocusMode): Enum indicating whether to autofocus or manually focus distance (float): Approximate distance to focus on, most accurate between 1.2m and 20m, only settable in PTZ_FOCUS_MANUAL mode focus_position (int32): Precise lens position for the camera for repeatable operations, overrides distance if specified, only settable in PTZ_FOCUS_MANUAL mode Returns: SetPtzFocusStateResponse indicating whether the call was successful """ ptz_focus_state = create_focus_state(focus_mode, distance, focus_position) request = ptz_pb2.SetPtzFocusStateRequest(focus_state=ptz_focus_state) return self.call(self._stub.SetPtzFocusState, request, self._set_ptz_focus_state_from_response, common_header_errors, copy_request=False, **kwargs)
[docs] def set_ptz_focus_state_async(self, focus_mode, distance=None, focus_position=None, **kwargs): """Async version of set_ptz_focus_state()""" ptz_focus_state = create_focus_state(focus_mode, distance, focus_position) request = ptz_pb2.SetPtzFocusStateRequest(focus_state=ptz_focus_state) return self.call_async(self._stub.SetPtzFocusState, request, self._set_ptz_focus_state_from_response, common_header_errors, copy_request=False, **kwargs)
@staticmethod def _list_ptz_from_response(response): return response.ptzs @staticmethod def _get_ptz_position_from_response(response): return response.position @staticmethod def _get_ptz_velocity_from_response(response): return response.velocity @staticmethod def _set_ptz_position_from_response(response): return response.position @staticmethod def _set_ptz_velocity_from_response(response): return response.velocity @staticmethod def _initialize_lens_from_response(response): return response # Focus methods @staticmethod def _get_ptz_focus_state_from_response(response): return response.focus_state @staticmethod def _set_ptz_focus_state_from_response(response): return response
[docs]def shift_pan_angle(pan): """Shift the pan angle (degrees) so that it is in the [0,360] range.""" return recenter_value_mod(pan, 180, 360)
[docs]def create_focus_state(focus_mode, distance=None, focus_position=None): """Generate a focus state proto.""" approx_distance = None focus_position_val = None if focus_mode == ptz_pb2.PtzFocusState.PTZ_FOCUS_MANUAL: if focus_position is not None: focus_position_val = Int32Value(value=focus_position) approx_distance = None elif distance is not None: approx_distance = FloatValue(value=distance) focus_position_val = None else: raise ValueError("One of distance or focus_position must be specified.") return ptz_pb2.PtzFocusState(mode=focus_mode, approx_distance=approx_distance, focus_position=focus_position_val)