Source code for bosdyn.mission.client

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""For clients to the mission service."""

import collections

from google.protobuf import timestamp_pb2

from bosdyn.api.mission import mission_pb2, mission_service_pb2_grpc
from bosdyn.client import data_chunk
from bosdyn.client.common import (BaseClient, common_header_errors, error_factory,
                                  handle_common_header_errors, handle_lease_use_result_errors,
                                  handle_unset_status_error)
from bosdyn.client.exceptions import ResponseError, TimeSyncRequired, UnimplementedError
from bosdyn.client.lease import add_lease_wallet_processors


[docs]class MissionResponseError(ResponseError): """General class of errors for mission service."""
[docs]class InvalidQuestionId(MissionResponseError): """The indicated question is unknown."""
[docs]class InvalidAnswerCode(MissionResponseError): """The indicated answer code is invalid for the specified question."""
[docs]class QuestionAlreadyAnswered(MissionResponseError): """The indicated question was already answered."""
[docs]class CustomParamsError(MissionResponseError): """The indicated answer does not match the spec for the indicated answer"""
[docs]class IncompatibleAnswer(MissionResponseError): """The indicated answer is not in a format expected by the indicated question."""
[docs]class CompilationError(MissionResponseError): """Mission could not be compiled."""
[docs]class ValidationError(MissionResponseError): """Mission could not be validated.""" def __init__(self, response, error_message=None): super(ValidationError, self).__init__(self, response) self.failed_nodes = response.failed_nodes def __str__(self): return 'Mission validation failed with: {}'.format('; '.join( [n.error for n in self.failed_nodes]))
[docs]class NoMissionError(MissionResponseError): """There is no mission to be played/restarted."""
[docs]class NoMissionPlayingError(MissionResponseError): """There is no mission to be paused."""
[docs]class MissionClient(BaseClient): """Client for the Mission service.""" default_service_name = 'robot-mission' service_type = 'bosdyn.api.mission.MissionService' def __init__(self): super(MissionClient, self).__init__(mission_service_pb2_grpc.MissionServiceStub) self._timesync_endpoint = None
[docs] def update_from(self, other): super(MissionClient, self).update_from(other) if self.lease_wallet: add_lease_wallet_processors(self, self.lease_wallet) # Grab a timesync endpoint if it is available. try: self._timesync_endpoint = other.time_sync.endpoint except AttributeError: pass # other doesn't have a time_sync accessor
@property def timesync_endpoint(self): """Accessor for timesync endpoint that was grabbed via 'update_from()'.""" if not self._timesync_endpoint: raise TimeSyncRequired return self._timesync_endpoint
[docs] def get_state(self, upper_tick_bound=None, lower_tick_bound=None, past_ticks=None, **kwargs): """Obtain current mission state. Raises: RpcError: Problem communicating with the robot. """ req = self._get_state_request(upper_tick_bound, lower_tick_bound, past_ticks) return self.call(self._stub.GetState, req, _get_state_value, common_header_errors, copy_request=False, **kwargs)
[docs] def get_state_async(self, upper_tick_bound=None, lower_tick_bound=None, past_ticks=None, **kwargs): """Async version of get_state()""" req = self._get_state_request(upper_tick_bound, lower_tick_bound, past_ticks) return self.call_async(self._stub.GetState, req, _get_state_value, common_header_errors, copy_request=False, **kwargs)
[docs] def answer_question(self, question_id, code=None, custom_params=None, **kwargs): """Specify an answer to the question asked by the mission. Args: question_id (int): ID of the question to answer. code (int): Answer code. custom_params (DictParam): Answer to a custom params prompt. Raises: RpcError: Problem communicating with the robot. InvalidQuestionId: question_id was not a valid id. InvalidAnswerCode: code was not valid for the question. QuestionAlreadyAnswered: The question for question_id was already answered. CustomParamsError: The answer did not match the spec for the question. IncompatibleAnswer: The answer did not match a type expected for the question. """ req = self._answer_question_request(question_id, code, custom_params) return self.call(self._stub.AnswerQuestion, req, None, _answer_question_error_from_response, copy_request=False, **kwargs)
[docs] def answer_question_async(self, question_id, code=None, custom_params=None, **kwargs): """Async version of answer_question()""" req = self._answer_question_request(question_id, code, custom_params) return self.call_async(self._stub.AnswerQuestion, req, None, _answer_question_error_from_response, copy_request=False, **kwargs)
[docs] def load_mission(self, root, leases=[], **kwargs): """Load a mission onto the robot. Args: root: Root node in a mission. leases: All leases necessary to initialize a mission. Raises: RpcError: Problem communicating with the robot. bosdyn.mission.client.CompilationError: The mission failed to compile. bosdyn.mission.client.ValidationError: The mission failed to validate. """ req = self._load_mission_request(root, leases) return self.call(self._stub.LoadMission, req, None, _load_mission_error_from_response, copy_request=False, **kwargs)
[docs] def load_mission_async(self, root, leases=[], **kwargs): """Async version of load_mission""" req = self._load_mission_request(root, leases) return self.call_async(self._stub.LoadMission, req, None, _load_mission_error_from_response, copy_request=False, **kwargs)
[docs] def load_mission_as_chunks(self, root, leases=[], data_chunk_byte_size=1000 * 1000, **kwargs): """Load a mission onto the robot. Args: root: Root node in a mission. leases: All leases necessary to initialize a mission. data_chunk_byte_size: max size of each streamed message Raises: RpcError: Problem communicating with the robot. bosdyn.mission.client.CompilationError: The mission failed to compile. bosdyn.mission.client.ValidationError: The mission failed to validate. """ req = self._load_mission_request(root, leases) self._apply_request_processors(req, copy_request=False) return self.call(self._stub.LoadMissionAsChunks, data_chunk.chunk_message(req, data_chunk_byte_size), None, _load_mission_error_from_response, **kwargs)
[docs] def load_mission_as_chunks2(self, root, leases=[], data_chunk_byte_size=1000 * 1000, **kwargs): """Load a mission onto the robot. Args: root: Root node in a mission. leases: All leases necessary to initialize a mission. data_chunk_byte_size: max size of each streamed message Raises: RpcError: Problem communicating with the robot. bosdyn.mission.client.CompilationError: The mission failed to compile. bosdyn.mission.client.ValidationError: The mission failed to validate. """ req = self._load_mission_request(root, leases) self._apply_request_processors(req, copy_request=False) return self.call(self._stub.LoadMissionAsChunks2, data_chunk.chunk_message(req, data_chunk_byte_size), error_from_response=_load_mission_error_from_response, assemble_type=mission_pb2.LoadMissionResponse, copy_request=False, **kwargs)
[docs] def play_mission( self, pause_time_secs, leases=[], settings=None, **kwargs): """Play the loaded mission. Args: pause_time_secs: Absolute time when the mission should pause execution. Subsequent RPCs will override this value, so you can use this to say "if you don't hear from me again, stop running the mission at this time." leases: Leases the mission service will need to use. Unlike other clients, these MUST be specified. Raises: RpcError: Problem communicating with the robot. NoMissionError: No mission Loaded. """ req = self._play_mission_request( pause_time_secs, leases, settings) return self.call(self._stub.PlayMission, req, None, _play_mission_error_from_response, copy_request=False, **kwargs)
[docs] def play_mission_async( self, pause_time_secs, leases=[], settings=None, **kwargs): """Async version of play_mission.""" req = self._play_mission_request( pause_time_secs, leases, settings) return self.call_async(self._stub.PlayMission, req, None, _play_mission_error_from_response, copy_request=False, **kwargs)
[docs] def restart_mission(self, pause_time_secs, leases=[], settings=None, **kwargs): """Restart the loaded mission. Args: pause_time_secs: Absolute time when the mission should pause execution. Subsequent RPCs to RestartMission will override this value, so you can use this to say "if you don't hear from me again, stop running the mission at this time." leases: Leases the mission service will need to use. Unlike other clients, these MUST be specified. Raises: RpcError: Problem communicating with the robot. NoMissionError: No Mission Loaded. bosdyn.mission.client.ValidationError: The mission failed to validate. """ req = self._restart_mission_request(pause_time_secs, leases, settings) return self.call(self._stub.RestartMission, req, None, _restart_mission_error_from_response, copy_request=False, **kwargs)
[docs] def restart_mission_async(self, pause_time_secs, leases=[], settings=None, **kwargs): """Async version of restart_mission.""" req = self._restart_mission_request(pause_time_secs, leases, settings) return self.call_async(self._stub.RestartMission, req, None, _restart_mission_error_from_response, copy_request=False, **kwargs)
[docs] def pause_mission(self, **kwargs): """Pause the running mission. Raises: RpcError: Problem communicating with the robot. NoMissionPlayingError: No mission playing. """ req = self._pause_mission_request() return self.call(self._stub.PauseMission, req, None, _pause_mission_error_from_response, copy_request=False, **kwargs)
[docs] def pause_mission_async(self, **kwargs): """Async version of pause_mission().""" req = self._pause_mission_request() return self.call_async(self._stub.PauseMission, req, None, _pause_mission_error_from_response, copy_request=False, **kwargs)
[docs] def stop_mission(self, **kwargs): """Stop the running mission. Raises: RpcError: Problem communicating with the robot. NoMissionPlayingError: No mission playing. """ req = self._stop_mission_request() return self.call(self._stub.StopMission, req, None, _stop_mission_error_from_response, copy_request=False, **kwargs)
[docs] def stop_mission_async(self, **kwargs): """Async version of stop_mission().""" req = self._stop_mission_request() return self.call_async(self._stub.StopMission, req, None, _stop_mission_error_from_response, copy_request=False, **kwargs)
[docs] def get_info(self, **kwargs): """Get static information about the loaded mission. Raises: RpcError: Problem communicating with the robot. """ req = self._get_info_request() try: return self._get_info_as_chunks_call(req) except UnimplementedError as err: # This indicates that the software release running on robot does not yet have # the implementation for the streaming response of GetInfo. return self.call(self._stub.GetInfo, req, _get_info_value, common_header_errors, copy_request=False, **kwargs)
def _get_info_as_chunks_call(self, req, **kwargs): """Issues the GetInfoAsChunks RPC to the mission service.""" return self.call(self._stub.GetInfoAsChunks, req, _get_info_value, error_from_response=common_header_errors, assemble_type=mission_pb2.GetInfoResponse, copy_request=False, **kwargs)
[docs] def get_info_async(self, **kwargs): """Async version of get_info.""" req = self._get_info_request() return self.call_async(self._stub.GetInfo, req, _get_info_value, common_header_errors, copy_request=False, **kwargs)
[docs] def get_mission(self, **kwargs): """Get the loaded mission. Raises: RpcError: Problem communicating with the robot. """ req = self._get_mission_request() try: return self._get_mission_as_chunks_call(req) except UnimplementedError as err: # This indicates that the software release running on robot does not yet have # the implementation for the streaming response of GetMission. return self.call(self._stub.GetMission, req, None, common_header_errors, copy_request=False, **kwargs)
[docs] def get_mission_async(self, **kwargs): """Async version of get_mission().""" req = self._get_mission_request() return self.call_async(self._stub.GetMission, req, None, common_header_errors, copy_request=False, **kwargs)
def _get_mission_as_chunks_call(self, req, **kwargs): """Issues the GetMissionAsChunks RPC to the mission service.""" return self.call(self._stub.GetMissionAsChunks, req, value_from_response=None, error_from_response=common_header_errors, assemble_type=mission_pb2.GetMissionResponse, copy_request=False, **kwargs) @staticmethod def _get_state_request(upper_tick_bound, lower_tick_bound, past_ticks): if lower_tick_bound is not None and past_ticks is not None: raise ValueError('Cannot specify both lower_tick_bound and past_ticks') request = mission_pb2.GetStateRequest(history_lower_tick_bound=lower_tick_bound, history_past_ticks=past_ticks) if upper_tick_bound is not None: request.history_upper_tick_bound.value = upper_tick_bound return request @staticmethod def _answer_question_request(question_id, code, custom_params): return mission_pb2.AnswerQuestionRequest(question_id=question_id, code=code, custom_params=custom_params) @staticmethod def _load_mission_request(root, leases): request = mission_pb2.LoadMissionRequest(root=root) for lease in leases: request.leases.add().CopyFrom(lease.lease_proto) return request def _play_mission_request( self, pause_time_secs, leases, settings): request = mission_pb2.PlayMissionRequest( pause_time=self.timesync_endpoint.robot_timestamp_from_local_secs(pause_time_secs), settings=settings) for lease in leases: request.leases.add().CopyFrom(lease.lease_proto) return request def _restart_mission_request(self, pause_time_secs, leases, settings): request = mission_pb2.RestartMissionRequest( pause_time=self.timesync_endpoint.robot_timestamp_from_local_secs(pause_time_secs), settings=settings) for lease in leases: request.leases.add().CopyFrom(lease.lease_proto) return request @staticmethod def _pause_mission_request(): return mission_pb2.PauseMissionRequest() @staticmethod def _stop_mission_request(): return mission_pb2.StopMissionRequest() @staticmethod def _get_info_request(): return mission_pb2.GetInfoRequest() @staticmethod def _get_mission_request(): return mission_pb2.GetMissionRequest()
def _get_state_value(response): return response.state def _get_info_value(response): if response.HasField(str('mission_info')): return response.mission_info return None _ANSWER_QUESTION_STATUS_TO_ERROR = collections.defaultdict(lambda: (MissionResponseError, None)) _ANSWER_QUESTION_STATUS_TO_ERROR.update({ mission_pb2.AnswerQuestionResponse.STATUS_OK: (None, None), mission_pb2.AnswerQuestionResponse.STATUS_INVALID_QUESTION_ID: (InvalidQuestionId, InvalidQuestionId.__doc__), mission_pb2.AnswerQuestionResponse.STATUS_INVALID_CODE: (InvalidAnswerCode, InvalidAnswerCode.__doc__), mission_pb2.AnswerQuestionResponse.STATUS_ALREADY_ANSWERED: (QuestionAlreadyAnswered, QuestionAlreadyAnswered.__doc__), mission_pb2.AnswerQuestionResponse.STATUS_CUSTOM_PARAMS_ERROR: (CustomParamsError, CustomParamsError.__doc__), mission_pb2.AnswerQuestionResponse.STATUS_INCOMPATIBLE_ANSWER: (IncompatibleAnswer, IncompatibleAnswer.__doc__), }) @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _answer_question_error_from_response(response): return error_factory(response, response.status, status_to_string=mission_pb2.AnswerQuestionResponse.Status.Name, status_to_error=_ANSWER_QUESTION_STATUS_TO_ERROR) _LOAD_MISSION_STATUS_TO_ERROR = collections.defaultdict(lambda: (MissionResponseError, None)) _LOAD_MISSION_STATUS_TO_ERROR.update({ mission_pb2.LoadMissionResponse.STATUS_OK: (None, None), mission_pb2.LoadMissionResponse.STATUS_VALIDATE_ERROR: (ValidationError, None), mission_pb2.LoadMissionResponse.STATUS_COMPILE_ERROR: (CompilationError, None), }) @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') @handle_lease_use_result_errors def _load_mission_error_from_response(response): return error_factory(response, response.status, status_to_string=mission_pb2.LoadMissionResponse.Status.Name, status_to_error=_LOAD_MISSION_STATUS_TO_ERROR) _PLAY_MISSION_STATUS_TO_ERROR = collections.defaultdict(lambda: (MissionResponseError, None)) _PLAY_MISSION_STATUS_TO_ERROR.update({ mission_pb2.PlayMissionResponse.STATUS_OK: (None, None), mission_pb2.PlayMissionResponse.STATUS_NO_MISSION: (NoMissionError, None), }) @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') @handle_lease_use_result_errors def _play_mission_error_from_response(response): return error_factory(response, response.status, status_to_string=mission_pb2.PlayMissionResponse.Status.Name, status_to_error=_PLAY_MISSION_STATUS_TO_ERROR) _PAUSE_MISSION_STATUS_TO_ERROR = collections.defaultdict(lambda: (MissionResponseError, None)) _PAUSE_MISSION_STATUS_TO_ERROR.update({ mission_pb2.PauseMissionResponse.STATUS_OK: (None, None), mission_pb2.PauseMissionResponse.STATUS_NO_MISSION_PLAYING: (NoMissionPlayingError, None), }) @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') @handle_lease_use_result_errors def _pause_mission_error_from_response(response): return error_factory(response, response.status, status_to_string=mission_pb2.PauseMissionResponse.Status.Name, status_to_error=_PAUSE_MISSION_STATUS_TO_ERROR) _STOP_MISSION_STATUS_TO_ERROR = collections.defaultdict(lambda: (MissionResponseError, None)) _STOP_MISSION_STATUS_TO_ERROR.update({ mission_pb2.StopMissionResponse.STATUS_OK: (None, None), mission_pb2.StopMissionResponse.STATUS_NO_MISSION_PLAYING: (NoMissionPlayingError, None), }) @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') @handle_lease_use_result_errors def _stop_mission_error_from_response(response): return error_factory(response, response.status, status_to_string=mission_pb2.StopMissionResponse.Status.Name, status_to_error=_STOP_MISSION_STATUS_TO_ERROR) _RESTART_MISSION_STATUS_TO_ERROR = collections.defaultdict(lambda: (MissionResponseError, None)) _RESTART_MISSION_STATUS_TO_ERROR.update({ mission_pb2.RestartMissionResponse.STATUS_OK: (None, None), mission_pb2.RestartMissionResponse.STATUS_NO_MISSION: (NoMissionError, None), mission_pb2.RestartMissionResponse.STATUS_VALIDATE_ERROR: (ValidationError, None), }) @handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') @handle_lease_use_result_errors def _restart_mission_error_from_response(response): return error_factory(response, response.status, status_to_string=mission_pb2.RestartMissionResponse.Status.Name, status_to_error=_RESTART_MISSION_STATUS_TO_ERROR)